Attributes (Preheat Pump Low OA Alarm) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The following table describes the attributes used by the Preheat Pump Low OA Alarm modules.

Table 1. Preheat Pump Low OA Alarm Attributes

Name

Type 1

Description

Default Value

Alarm

 

Represents the Alarm condition of the pump, when in alarm and the OA-T is less than the OA Low SP. The output is in Alarm.

Normal

Set Name: Normal/Alarm

Differential

G, V

Specifies the differential for the OA compare.

0 °F

OA Low Setpoint

 

Represents the Low Outdoor Air Temperature Setpoint.

0 °F

OA Temperature

 

Represents the Outdoor Air Temperature.

0 °F

Output

 

Represents the current output of the module.

Normal

Set Name: Normal/Alarm

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)