Primary States (Latching Alarm Manager) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
  • When the Setup X attribute is set to Automatic, the Output is Alarm if the associated input is Alarm, and equals Normal when all input values are Normal.

  • When the Setup X attribute is set to Manual, the Output is Alarm if the associated input is Alarm, and equals Normal when all input values are Normal and the Reset X input is set to Reset.

Table 1. Latching Alarm Manager Command Hierarchy

Input

Reset

LastOut

Setup

Output

Alarm

*

*

*

Alarm

Normal

*

*

Automatic

Normal

Reset

Normal

Manual

Normal

Alarm

Manual

Normal

Off

Normal

Manual

Normal

Alarm

Manual

Alarm