Latching Alarm Manager - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

This module provides the ability to latch the inputs to the module. The module applies the OR operator to the result and passes it to the output. The Latching Alarm Manager module contains an input that attaches the OR operator to all of the results to cascade multiple modules.

When the Setup attribute is set to Automatic, the Output is Alarm when the value of any of the inputs is Alarm, and equals Normal when all input values are Normal.

When the Setup attribute is set to Manual, the Output is Alarm when the value of any of the inputs is Alarm, and equals Normal when all input values are Normal and the Reset input is set to Reset.

You can view and modify the modules in this group’s logic.