Viewing the State Table - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

During a commissioning or simulation session, the state table displays the active State Generation Module and shows the active state in each associated column of the Output Controllers. While a simulation session is running, Network Inputs to the State Generators can be overridden, and the results of the overrides to the Output Controllers can be seen in the state table view.

If you are using the Classic view, click the State Tables tab. If you are using a Perspective, add or view the State Tables widget.