Starting Simulation - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

Procedure

  1. Click Simulate. The Simulation dialog box appears.
  2. In the Startup Value section, select the simulation parameters or attributes.
  3. In the Speed x Realtime section, select the speed of the simulation. You can select between 1 (real time) and 10 (ten times real time).
  4. Click OK.
    Note: When simulating a VAV box, verify SA-VP is set to zero. Once Autocalibration is complete, the SA-VP can be increased to simulate airflow.