See the Starting Simulation section.
Field |
Description |
---|---|
Startup Value |
Startup values for the inputs of the application. |
Item |
Name of the item. |
Value |
Item’s starting value. |
Units |
Item’s starting units. |
Speed x Realtime |
Use to indicate the speed of the simulation. The speed range is 1–10 times real time. |
Starting Simulation Engine Status Bar |
Indicates the progress of entering Simulation mode. |
OK |
Starts simulation and closes the dialog box. |
Cancel |
Closes the screen without applying the changes. |
|
Opens the Help system. |