Debugging - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
Debugging functionality in simulation allows you to validate your logic.

When you start a simulation session, the Simulation Control Bar appears. The Control Bar is a convenient way to to control and view details about break conditions. Click View Break Conditions in the control bar to define break conditions, update break conditions, and delete break conditions.