Create State Selection to Interlock this Side Loop - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The selection options for Create State Selection to Interlock this Side Loop are:

  • Create State Selection to Interlock this Side Loop: This option adds a State Selection table interlock for this side loop.

  • Create New Input for Interlock: This option loads a XXX SLINT-S (Sideloop Interlock Status) Network Input or Binary Input to connect to the State Table.

    • Binary Input

    • Network Input