Setting Default System Selection Preferences - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
For information on the System Selection tree types, see the Applications section. For information on the System Selection Wizard, see System Selection Wizard in the Configuring a System section.

To set default System Selection preferences:

  1. On the Settings menu, click System Selection. The Preferences - System Selection screen appears. The left pane contains the different System Selection trees available. See the Preferences - Naming and Signal section.

  2. Navigate to and select the System Selection tree to modify. The tree appears in the right pane of the screen.

  3. Select and remove selections to fit your specific needs. The options you choose here determine how the tree appears in the System Selection Wizard when you add a new system or make changes to an existing system’s selections. Make selections by:

    • selecting a check box to turn a setting on and clearing a check box to turn a setting off

    • clicking an option button to select that item from among several possible options

    Note:

    To return to the original Johnson Controls standard preferences, use the Reset option. See the Resetting System Selection Preferences section.

  4. Click OK.