Reliability (Sideloop Maximum Selector) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English
Table 1. Sideloop Maximum Selector Reliability

Input

Behavior When Input Is Not Reliable

Input 1

The last Reliable value is used in the maximum selection.

Input 2

The last Reliable value is used in the maximum selection.