Attributes (Sideloop Average Inputs) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
Table 1 describes the attributes used by the Sideloop Average Inputs modules.

Table 1. Sideloop Average Inputs Attributes

Name

Type 1

Description

Default Value

Input 1

 

Contains the first input to be averaged.

0.0

Input 2

 

Contains the second input to be averaged.

0.0

Present Value

G, V

Average of the inputs.

 
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)