Module Use in Applications (VAV Dual Duct Minimum Flow Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The application System Selection trees use the individual modules in this group using the names in Table 1.

Table 1. VAV Dual Duct Minimum Flow Determination Uses in Application System Selection Trees

Module Instance Name

Applications

Minimum Flow Determination - Dual Duct

VAV Dual Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.