Attributes (VAV Dual Duct Minimum Flow Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
Table 1 describes the attributes used by the VAV Dual Duct Minimum Flow Determination modules.

Table 1. VAV Dual Duct Minimum Flow Determination Attributes

Name

Type 1

Description

Default Value

CD-MINFLOW (CD Min Flow)

G, V

Contains the minimum required cold deck flow.

0 l/s, 0 cfm

CDUNOCC-MINFLOW (Unocc CD Min Flow)

 

Contains the minimum required cold deck flow when unoccupied.

0 l/s, 0 cfm

CLDWNCD-MINFLOW (Cooldown CD Min Flow)

 

Contains the minimum required cold deck flow when cooldown.

0 l/s, 0 cfm

CLDWNHD-MINFLOW (Cooldown HD Min Flow)

 

Contains the minimum required hot deck flow when cooldown.

0 l/s, 0 cfm

HD-MINFLOW (HD Min Flow)

V

Contains the minimum required hot deck flow.

0 l/s, 0 cfm

HDUNOCC-MINFLOW (Unocc HD Min Flow)

 

Contains the minimum required hot deck flow when unoccupied.

0 l/s, 0 cfm

Occ CD Min Flow

 

Contains the minimum required cold deck flow when occupied.

0 l/s, 0 cfm

Occ HD Min Flow

 

Contains the minimum required hot deck flow when occupied.

0 l/s, 0 cfm

Occupancy

 

Contains the current Occupancy status of the unit.

Occupied

Set Name: Occ Effective

WarmupCooldown

 

Contains the current WarmupCooldown status of the unit.

Normal

Set Name: OST Warmup Cooldown

WUCD-MINFLOW (Warmup CD Min Flow)

 

Contains the minimum required cold deck flow when warmup.

0 l/s, 0 cfm

WUHD-MINFLOW (Warmup HD Min Flow)

 

Contains the minimum required hot deck flow when warmup.

0 l/s, 0 cfm

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)