Attributes (Temperature Request Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The following table describes the attributes used by the Temperature Request Determination module.

Table 1. Temperature Request Determination Attributes

Name

Type 1

Description

Default Value

CD Percent

 

Represents the cooling damper command.

0% open

Cooling Request

G

Indicates the output of the module:
  • 1: lower temperature supply air is required
  • 0: lower temperature supply air is not required

0

Cooling Setpoint

 

Indicates the maximum damper command that initiates a decrease in supply temperature.

95% open

Differential

 

Indicates the required reduction in damper command before pressure request is no longer required.

10%

HD Percent

 

Represents the heating damper command.

0% open

Heating Request

 
Indicates output of module:
  • 1: higher temperature supply air is required
  • 0: higher temperature supply air is not required

0

Heating Setpoint

 

Indicates the maximum damper command that initiates an increase in supply temperature.

95% open

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)