This module calculates the setpoint offset based on the outdoor air temperature. The Setpoint Reset by OA-T module has an input for the outdoor air temperature, two inputs for the outdoor air setpoints (OA High Setpoint and OA Low Setpoint), and two inputs for the offset span (Setpoint and Setpoint Span). The output of this module is the Setpoint Offset.
You can view and modify the modules in this group’s logic.