Discharge Air Setpoint Determination - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The Discharge Air Setpoint Determination module sets the DA-T Setpoint based on the operating modes of the air handler. The module accepts as input the Unoccupied Status, the WarmupCooldown state, the occupied setpoint, the unoccupied heating and cooling setpoints, and a default DA-T setpoint. The EFFDAT-SP (Discharge Air Setpoint) is set to the Occ Setpoint, the DATHTGUNOCC-SP (Unocc Heating Setpoint), or the DATCLGUNOCC-SP (Unocc Cooling Setpoint) based on the WarmupCooldown input first, and the Unocc Status input if WarmupCooldown does not equal Warmup or Cooldown.

You can view and modify the modules in this group’s logic.