Module Use in Applications (Minimum Flow Calculation) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Minimum Flow Calculation Uses in Application System Selection Trees

Module Instance Name

Applications

Min HW Flow Calculation

Central Heating Applications

To see a module's connections and how modules interact with it, view the Connections table.