Minimum Flow Calculation - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The Minimum Flow Calculation module provides a minimum flow value based on the number of running devices. This module provides a float output. Based on the inputs, the module sets the Output equal to the Min Flow or the sum of the devices currently running, whichever is larger.