Attributes (Flow Sum Calculation) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

Table 1 describes the attributes used by the Flow Sum Calculation module.

Table 1. Flow Sum Calculation Attributes

Name

Type 1

Description

Default Value

Contributing Flow 1

 

Measured flow to be added to Contributing Flow 2.

0 l/s, 0 cfm

Contributing Flow 2

 

Measured flow to be added to Contributing Flow 1.

0 l/s, 0 cfm

DA-F, SA-F, or FLOW (Calculated Flow)

G, V

Contains the result of the addition with reliability.

Display Units: l/s, cfm

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), DC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)