Attributes (Flow Differential Calculation) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

Table 1 describes the attributes used by the Flow Differential Calculation module.

Table 1. Flow Differential Calculation Attributes

Name

Type 1

Description

Default Value

CD-F, HD-F, or FLOW (Calculated Flow)

G, V

Contains the result of the subtraction with reliability.

Display Units: l/s, cfm

Contributing Flow

 

Measured flow to be subtracted from the Total Flow.

0 l/s, 0 cfm

Total Flow

 

Measured total flow.

0 l/s, 0 cfm

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)