Attributes (Unocc Heating Fan Lockout) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
Table 1 describes the attributes used by the Unocc Heating Fan Lockout module.

Table 1. Unoccupied Heating Fan Lockout Attributes

Name

Type 1

Description

Default Value

Heating isAvailable

 

Provides a network input used to enable or disable heating.

False

Heating Required

 

Indicates whether there is a need for heating.

True

Occupancy

 

Indicates the effective occupancy command.

Occupied

Set Name: Occ Effective

Preheat isAvailable

 

Provides a network input used to enable or disable the preheat functionality.

False

Present Value

 

Indicates the current status of the device availability. The Present Value is True when the device is available and False when the device is not available.

False

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)