Attributes (Unocc Cooling Fan Lockout) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

Table 1 describes the attributes used by the Unocc Cooling Fan Lockout module.

Table 1. Unoccupied Cooling Fan Lockout Attributes

Name

Type 1

Description

Default Value

Cooling isAvailable

 

Provides a network input used to enable or disable cooling.

False

Cooling Required

 

Indicates whether there is a need for cooling.

True

Occupancy

 

Indicates the effective occupancy command.

Occupied

Set Name: Occ Effective

Present Value

 

Indicates the current status of the device availability. The Present Value is True when the device is available and False when the device is not available.

False

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)