Module Use in Applications (SummerWinter Mode Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The application System Selection trees use individual modules in this group using the names in Table 1.

Table 1. SummerWinter Mode Determination Uses in Application System Selection Trees

Module Instance Name

Applications

Summer Winter Mode Determination

AHU Mixed Air Single Duct Applications

AHU 100% Outdoor Air Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.