Table 1 describes the attributes used by the Staged Device Enable Determination Parallel module.
Name |
Type 1 |
Description |
Default Value |
---|---|---|---|
Fan Mode |
Last command sent to the fan. |
Off Set Name: Off/On |
|
STGDEV-STATE (State) |
G, V |
Current effective status for the staged device. |
Enable Set Name: False/True/Fault |
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)