Attributes (Flow Status Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
Table 1 describes the attributes used by the Flow Status Determination module.

Table 1. Flow Status Determination Attributes

Name

Description

Default Value

Air Proving Switch

Current status of the Air Proving Switch.

Off

Set Name: Off/On

Delay

Specifies the delay allowed for the fan to start before a fault occurs.

30 Seconds

Fan Mode

Provides the last command sent to the fan.

Off

Set Name: Off/On

Fan Status

Current effective status of the Airflow Proving Switch. This attribute is the same as the Status except that Fault is mapped to False.

 

FLOW-S (Status)

Current effective status of the Airflow Proving switch.

Set Name: False/True/Fault

See Primary States (Flow Status Determination).