Module Use in Applications (Dual Fan Command OR) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Dual Fan Command OR Uses in Application System Selection Trees

Module Instance Name

Application

Dual Fan Command OR

AHU Mixed Air Single Duct Applications

AHU100% Outdoor Air Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.