Attributes (Subtract) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The following table describes the attributes used by the Subtract modules:

Table 1. Subtract Attributes

Name

Type 1

Description

Default Value

CHWTEMP-DIFF or CHWFLOW-DIFF [Output (Float)]

V

Indicates the differential of Input 2 subtracted from Input 1.

0

Input 1

 

Indicates the floating variable from which Input 2 is subtracted.

0

Input 2

 

Indicates the variable that is subtracted from Input 1.

0

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)