Module Use in Applications (PCHWP dP Setpoint Reset By Coil Position) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. PCHWP dP Setpoint Reset By Coil Position Uses in Application System Selection Trees

Module Instance Name

Applications

PCHWP dP Setpoint Reset By Coil Position

Central Cooling with Optimization Applications

SCHWP dP Setpoint Reset By Coil Position

Central Cooling with Optimization Applications

To see a module's connections and how modules interact with it, view the Connections table.