Load Filter - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The Load Filter module provides a digital filtered value for use within a Control Sequence.

The module has four main inputs:

  • Enable: When True, the Filter calculates a digital filtered value for the output after the Startup Delay time passes. When False, the input passes directly to the output.
  • Filter Enable: When On, the Filter calculates a digital filtered value for the output. When Off, the input passes directly to the output.
  • Input: Provides a floating point value and is typically connected from another block.
  • Time Constant: Determines the cutoff frequency and the execution period.

You can view and modify the modules in this group’s logic.