Module Use in Applications (Device Alarm) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Device Alarm Uses in Application System Selection Trees

Module Instance Name

Applications

CHW Pmp X Alarm (Where X Is 1-8)

Central Cooling with Optimization Applications

CW Pmp X Alarm (Where X Is 1-8)

Central Cooling with Optimization Applications

Cooling Tower X Alarm v51 (Where X Is 1-8)

Central Cooling with Optimization Applications

Secondary Pump X Alarm (Where X Is 1-8)

Central Cooling with Optimization Applications

To see a module's connections and how modules interact with it, view the Connections table.