Module Use in Applications (Chiller Percent Load Setpoint Reset) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Chiller Percent Load Setpoint Reset Uses in Application System Selection Trees

Module Instance Name

Applications

Chiller Percent Load Setpoint Reset

Central Cooling with Optimization Applications

To see a module's connections and how modules interact with it, view the Connections table.