Chiller Percent Load Setpoint Reset - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

The Chiller Percent Load Setpoint Reset module provides the Upper and Lower Percent Load Setpoints for the Chiller Selector. This module provides two float outputs, one for the Upper Percent and another for the Lower Percent setpoint. Based on the inputs, the module spans the Outputs between a high and low range. This module is implemented as a Hybrid activity.

Figure 1. Chiller Percent Load Setpoint Reset