Chiller Forced Upstage - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The Chiller Forced Upstage module derates the current running chillers by comparing the CHW supply temp and flow to a setpoint. This module provides two Boolean outputs. One output sets the derate flag true or false based on its inputs. The other output issues a 5-second derate reset pulse 5 minutes after the derate flag transitions from true to false. This module is implemented as a control activity.

Figure 1. Chiller Forced Upstage