Capacity Calculation - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Capacity Calculation module may be used to sum device amperes, device flow, or pump flow. The calculation can be a function of measured data or rated data. This module accepts inputs for rated capacities or pump flows, running capacities, and device usage. The module calculates the operating capacity and available capacity.

You cannot view and modify modules in this group’s logic.