Procedure
- In the Perspective Management dialog box, select the Table Data widget you want to configure.
- Enter a Name and Description (optional) for the Table Data widget. The name appears in the UI, and the description appears as a tooltip when you hover over the component in the UI.
- Click the Data Criteria Type drop-down box and select UI Column.
- Select the Visible check box to show the widget within the UI, or clear the check box to hide the widget in the UI.
- Click the Order drop-down box and select whether you would like the table data to appear in Alphabetical order or As Defined. (See Figure 1 in Table Data for examples.)
-
In the selection window, select one or more categories (UI Columns) you would like to display in the Table Data widget. To select multiple categories, press and hold down the Ctrl key and click each category you would like to display.
Note: When you select As Defined for Order and State Generation UI Column, the blocks appear in the same order as the State Table.
- Click Apply.
- If you create multiple Table Data widgets and want to organize them within the perspective UI, nest the group of Table Data widgets within a Tab or Orientation container. See Adding a Container for more information.