Table Data Widget - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The following table provides information on selections found in the table data custom configuration panel.

Table 1. Table Data Widget
Field Description
Name

Indicates the name that appears within the perspective UI.

Description

Indicates the text included in the tooltip that appears within the UI when you hover over the widget's header.

Data Criteria Type

UI Column: Enables you to select table data from a set of UI Column types.

BACoid: Enables you to specify table data by BACoid.

Visible Indicates if the widget appears within the UI.
Order

Alphabetical: Specifies that table data appears in alphabetical order.

As Defined: Specifies that table data appears in the order you defined the data. This order type applies more to the BACoid data criteria type.

Note: When you specify that State Generator table data (UI Column) appear As Defined, the State Generator table data appears in the same order as the State Table.
Settings - Show All When selected, shows all points within the application. When cleared, shows only BACnet Exposed points.
Note: This attribute appears only when you have an application open.
Expansion Level Indicates the level of details that appear within the tree (1 to 5).
Note: This attribute appears only when you have an application open.
Filter Provides a text box to search the selection tree based on the node name. The search results include the matching node and its ancestors.
Moves a subcomponent up in the display order. Applies when the Order property is set to As Defined.
Note: This attribute appears only when you have an application open.
Moves a subcomponent down in the display order. Applies when the Order property is set to As Defined.
Note: This attribute appears only when you have an application open.
Object Identifier Allows the user to manually define a BACoid to display in the widget.
Adds the manually defined Object Identifier to the widget's list of BACoids.
Removes the manually defined Object Identifier to the widget's list of BACoids.
Removes the selected points in the list from the widget.
Adds the selected points in the list to the widget.