Parameters - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

The Parameters widget appears in Features Panel of the Classic View workspace and in the Application Tab of the Simple View workspace, in all modes. The Parameters widget lists key parameters/attributes in alphabetical order used by the system. In Configuration mode, default values appear only for parameters/attributes that can be edited. To add other parameters/attributes to the Parameters table, enable the inputs and outputs for BACnet network exposure by editing the individual module’s BACnet Exposed attribute to True in the Details dialog box. You cannot modify outputs of modules from the Parameters table. See the Features Panel Screen section for a description of this table’s components.

Note: You cannot modify outputs of modules from the Parameters table.
Table 1. Parameters Widget

Screen Area

Description

Edit Enters Edit mode and allows modification of default parameter/attributes values.
Apply Saves the changes to parameter/attributes values.
Cancel Cancels the edits made and exits Edit mode.
Item Lists the names of the parameters/attributes.
Current Value Current calculated values of the parameters/attributes (Simulation and Commissioning modes only).
Default Value Default values of the parameters/attributes.
Units Units of measurement used for the parameters/attributes.
Standard Name Displays descriptive text for the parameters/attributes.