Connections - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Connections table appears in the Connection tab of the Features Panel in all modes. This table can show the connections for one or more modules and the State Selection tables. The Connections table displays the source and destination module and port data with the associated input and output connection of the selected module. In this table, inputs appear yellow and outputs appear turquoise.

In the Control tab, you can select to view connections for one module, multiple modules in a module category, State Selector only, or you can click Show All to view all connections.

In the Logic tab, you can select a module in the Activities tree to view the connections for the selected module. You can also select a module in the BACnet Exposed tab to view and update the Connections table.

Note: Select the Freeze Connection check box to prevent the Connections table from dynamically changing as you select modules.
Figure 1. Connections Table Show All Menu