Widget - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
Widgets are items that display specific information and include specific functional behaviors. The Classic View perspective includes all of the following widgets, except for the System Selection Information widget.

Note: The Advanced Data, BACnet Exposed, Connections, Local Display, Logic View, Parameters, State Tables, and System Selection Information widgets are known as specialized widgets because they have no configurable data.
Table 1. Widget
Icon Section Property Selection
Specialized widget that allows you to view and work with advanced controller information. See Advanced Data widget.

Visible

Specialized widget that allows you to view and work with points in the application. See BACnet Exposed widget.

Visible

Specialized widget that allows you to view and work with connections of the Control Sequence. See Connections widget.

Visible

Configurable widget that allows you to view the details of a BACoid (BACnet Object ID). See Details Data widget and Data Criteria.

Data Criteria Type

Visible

Specialized widget that allows you to view and configure the display device. See Display widget.

Visible

Specialized widget that allows you to view and work with application logic. See Logic View widget.

Visible

Specialized widget that allows you to view parameters. See Parameters widget.

Visible

Specialized widget that allows you to view and work with State Table information. See State Tables widget.

Visible

Specialized widget that allows you to view system design information. See System Selection Information widget.

Visible

Configurable widget that allows you to select and display multiple BACoids using data criteria. See Table Data widget and Data Criteria.

Data Criteria Type

Visible

Order