The following table shows how the Simple View is broken into components of a perspective.
Simple View Component | Type | Orientation/ Location/ Data Criteria | Direct Subcomponents | Appearance Description |
---|---|---|---|---|
Entire Simple View | Tab Container | Top |
Orientation Container (Application) System Selection Information Widget (System Selection Information tab) |
The Simple View is a tab container that specifies that the two subcomponents appear as tabs. |
Application Tab | Orientation Container | Horizontal |
Table Data Widget - UI Column (Inputs column) Parameters Widget (Parameters column) Table Data Widget - UI Column (Outputs column) |
The orientation container type specifies that the three subcomponents be arranged horizontally, or stacked next to each other. |
Inputs | Table Data Widget | UI Column | None | The Table Data widget with UI Column data criteria specifies that Miscellaneous Inputs, Network Inputs, and Sensors appear within the same table in the UI. |
Parameters | Parameters Widget | Not Applicable | None | The parameters widget displays application parameters and cannot be configured. |
Outputs | Table Data Widget | UI Column | None | The Table Data widget with UI Column data criteria specifies that Control Points, Miscellaneous Outputs, and Network Outputs appear within the same table in the UI. |
System Selection Information Tab | System Selection Information Widget | Not Applicable | None | The System Selection Information widget displays system selection choices and cannot be configured. |