Adding Objects Using Auto-Discovery - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

Procedure

  1. Log on to the NAE, and view the FC Bus object in the Focus Window.
  2. Select the Engineering tab.
  3. Use the Integration Tree to and find the object you want to add. For example, if you want to add a Cooling PID attribute PRAC Status, open the control application in the tree, the output module that contains the PID, an activity in the module that contains the PID, and then the PID. All attributes of the PID appear, including PRAC Status.
  4. Double-click the object. Object details appear in the right pane.
  5. Click Edit and locate the BACnet Exposed attribute.
  6. In the drop-down list next to BACnet Exposed, click True. Click Save.
  7. You can now use auto-discovery to add the object to the NAE online using the Insert Field Point Wizard, and select Assisted Point Definition to invoke auto-discovery. Refer to the Insert Point Wizard section in the Metasys system Help (LIT-1201793) for details.