Attributes (Sideloop Reset Output) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The following table describes the attributes used by the Sideloop Reset Output module.

Table 1. Sideloop Reset Output Attributes

Name

Type 1

Description

Default Value

Input

 

Used to reset the desired setpoint for the process variable to be controlled to when commanded to Control.

0.0

Mode

 

Allows the state to be set to Min, Max, or Control.

Control

Set Name: Min/Max/Control

Present Value

V

Contains the result of spanning the Input using the Input Range Low, Input Range High, Output Range Low, and Output Range High.

 

SL-OUTA (Output Range Low)

 

Used to set up the span when the mode is Control. This represents the Present Value when the Input is at or below the Input Range Low.

0.0

SL-OUTB (Output Range High)

 

Used to set up the span when the mode is Control. This represents the Output when the Input is at or above the Input Range High.

0.0

SL-OUTSTATE (State)

G, V

Current State of the module.

Set Name: Min/Max/Control

SL-RSTA (Input Range Low)

 

Used to set up the span when the mode is Control. This corresponds to the low x value.

0.0

SL-RSTB (Input Range High)

 

Used to set up the span when the mode is Control. This corresponds to the high x value.

0.0

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)