Sideloop Reset Output - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English

This module spans the input using coordinates of a straight line. The Output is the result of the span. The module accepts as inputs, a mode, an input, input range low, input range high, output range low, and output range high. The module outputs a value based on the input mode and parameter settings.

You can view and modify the modules in this group’s logic.

To see a module's connections and how modules interact with it, view the Connections table.