Primary States (Sideloop PI Proportional Output) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
  • Off: Set the Percent Cmd to 0%.

  • Max: Set the Percent Cmd to 100%.

  • Control: Adjust the Percent Cmd to control the Process Variable. If the Process Variable is reliable, the module controls the Percent Cmd to maintain the process variable at the Setpoint.

  • Hold: Holds the Percent Cmd output at its current value. If the Output Overridden input is true, then the Output Position input passes to the Percent Cmd.