Module Use in Applications (Sideloop PI Proportional Output) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Sideloop PI Proportional Output Uses in Application System Selection Trees

Module Instance Name

Applications

Chilled Water Bypass Valve Control v51

Central Cooling Applications

CHW Pump Differential Pressure Control v51

Central Cooling with Optimization Applications

Condenser Water Bypass Valve Control v51

Central Cooling Applications

Cooling Tower Control v51

Central Cooling Applications

Hot Water Bypass Valve Control v51

Central Heating Applications

Modulating Device PID v51

Central Cooling Applications

PI Proportional Output v51

Sideloop Applications

To see a module's connections and how modules interact with it, view the Connections table.