Primary States (Sideloop Interlock Binary to Binary) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English
  • Off: The Present Value is set to Off.

  • On: The Present Value is set to On.

  • Control: If the Input is On and all timers are satisfied, the Present Value is set to On. If the input is Off and all timers are satisfied, the Present Value is set to Off.