The following table describes the attributes used by the Sideloop Interlock Binary to Analog module.
Name |
Type 1 |
Description |
Default Value |
---|---|---|---|
Input |
Contains the input to this module. |
Off Set Name: Off/On |
|
Mode |
Contains a connection to the Selection object of a control System. It overrides the internal logic. |
Control Set Name: Off/On/Control |
|
Present Value |
G, V |
Analog value output based on the input and the status of the associated delays. |
|
SL-DELAYTYPE (Delay Type) |
Selects the type of delay from the time the binary input is energized or de-energized to the time when the analog output goes to Output Range High or Output Range Low. This can be set for None, On, Off, or Both. |
None Set Name: BI to BO/AO Delay Type |
|
SL-OFFDELAY (Off Delay) |
Specifies the delay from the time the input is de-energized to the time when the analog output goes to Output Range Low. |
30 Seconds |
|
SL-ONDELAY (On Delay) |
Specifies the delay from the time the binary input is energized to the time when the analog output goes to Output Range High |
30 Seconds |
|
SL-OUTA (Output Range Low) |
Contains the value sent to the output when the input is off and all timers are satisfied. If the Mode is Off, this value is sent to the Output. |
0.0 |
|
SL-OUTB (Output Range High) |
Contains the value sent to the output when the input is on and all timers are satisfied. If the Mode is On, this value is sent to the Output. |
100.0 |