Reliability (Sequencer) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Language
English
  • The reliability associated with the Sequencer module may report the input unreliable. When the input is unreliable, all outputs hold the last value set when the input was reliable during this situation.

  • If the Sequencer is unable to stage up or down because the remaining outputs are disabled, the Sequencer’s reliability is Unreliable.