Reliability (Zone Damper w Proportional Heating Valve) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Table 1. Zone Damper w Proportional Heating Valve Reliability

Input

Behavior When Input Is Not Reliable

Process Variable

Damper action set based on the Unreliable Option input.