The application System Selection trees use the individual modules in this group using the names in the following table.
Module Instance Name |
Applications |
---|---|
Zone X with Proportional Heating Valve Control v51 (Where X Is 1-8) |
To see a module's connections and how modules interact with it, view the Connections table.